SBOU307 October   2024

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   5
  6. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  7. 2Hardware
    1. 2.1 Quick Start Setup
    2. 2.2 EVM Operation
      1. 2.2.1 Current Sensing Operation
        1. 2.2.1.1 Detailed Setup
    3. 2.3 Circuitry
      1. 2.3.1 Current Sensing IC
      2. 2.3.2 Input Signal Path
      3. 2.3.3 Digital Circuitry
    4. 2.4 PAMB Compatibility
  8. 3Software
    1. 3.1 Setup
      1. 3.1.1 Driver Installation
      2. 3.1.2 Firmware
        1. 3.1.2.1 Firmware Debug
      3. 3.1.3 GUI Setup and Connection
        1. 3.1.3.1 Initial Setup
        2. 3.1.3.2 GUI to EVM Connection
    2. 3.2 GUI Operation
      1. 3.2.1 Home Tab
      2. 3.2.2 Registers Tab
      3. 3.2.3 Results Data Tab
    3. 3.3 Direct EVM USB Communication
      1. 3.3.1 Standard USB Read and Write Operations
      2. 3.3.2 Collect Data Through the USB BULK Channel
  9. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layout
    3. 4.3 Bill of Materials
  10. 5Additional Information
    1. 5.1 Trademarks
  11. 6Related Documentation From Texas Instruments

GUI to EVM Connection

To connect the GUI to the EVM, follow these steps:

  1. Setup and launch the GUI as described in Initial Setup.
    1. Make sure to connect the EVM to the SCB before powering on.
  2. Close the README.md file page to initiate a connection between the EVM and the GUI. If successful, then the text Hardware Connected is visible near the bottom left corner of the GUI.
    INA260EVM Hardware ConnectedFigure 3-4 Hardware Connected
    1. A green indicator with the device type and the text DEVICE CONNECTED is also visible near the top left of the GUI.
      INA260EVM Device ConnectedFigure 3-5 Device Connected
    2. If Hardware Connected and DEVICE CONNECTED do not show in the GUI, then long-press the RESET button on the EVM to try again.
      1. If that option does not work, then check different hardware COM ports under Options > Serial Port.
        INA260EVM Change Serial PortFigure 3-6 Change Serial Port
    3. If the hardware still does not connect, then make sure the correct GUI and EVM combination is being used.
      1. If you are using the correct GUI and EVM combination, then you may need to reprogram the firmware of the SCB, as described in Firmware Debug.
      2. Many connectivity issues can be addressed by doing one of the following:
        1. Long-press the RESET button on the EVM with the EVM and SCB connected to each other.
          • Refreshing the GUI can also sometimes help this.
        2. Connect the EVM to a different USB port.
          • Avoid using long cables and USB hubs.
          • If using a desktop PC, try a USB port on the back.