To view and edit the device registers, click the
(Registers) icon
on the menu to the left. The Registers tab looks like the one shown in Figure 3-8.
From this page, you can read and write device registers on the EVM. Here are some important notes:
- Use the Selected EVM drop-down menu at the top to choose which device to work with on the Registers page.
- Note, changing this here also changes the same setting for the Configuration tab.
- Functionally, this setting sets the default read/write address in the MCU
and then reads all register values back to update the Registers page.
Note that if data is being collected at a high frequency, then this can
cause a minor delay in the data collection. To prevent this, set device
settings before you start collecting data.
- By default, all changes are automatically written
to the device. If desired, then change the Immediate Write setting to
Deferred Write to only allow writing when ready.
- The user can modify writable register values from
any of these methods:
- Through the widget settings in the Field
View section on the right.
- Changing the Value directly with
either hex or decimal values.
- Double-clicking on any individual bit.
- Turning on Auto Read only updates registers in the Registers page, and not the plots in the Results Data section.
- Leaving Auto Read on while collecting data for plots can interfere with data collection timing.
- For questions about a register or register bit field, select the
icon.- For even more questions about registers, check the data sheet.
- For convenience, register settings can be saved and loaded back later to any device with the same register map. To do this, go to File > Register Data, as shown in Figure 3-9.
- Press the Read All Registers button after loading data to update the Registers page with the actual device values in case the loaded registers were not compatible with the connected device.