If desired, then this EVM and GUI
can be used with the PAMB Controller (DC081A) by jumper wiring the pin headers of the
PAMB to the EVM.
Figure 2-4 shows which pins on
the PAMB correspond to the EVM header pins. Note not to add too much resistance in the
jumper wire connection setup or the signal can degrade and cause communication
errors.