SBOU328 May 2025
To use the EVM with the SCB Controller (sold separately), connect the EVM as shown in Figure 2-1.
If using multiple EVMs, then connect as shown in Figure 2-2. Make sure to use a different address for each device. The GUI only supports one EVM and device type at a time; up to four EVMs total.