SBOU328 May   2025

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   5
  6. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  7. 2Hardware
    1. 2.1 Quick Start Setup
    2. 2.2 EVM Operation
      1. 2.2.1 Current Sensing Operation
        1. 2.2.1.1 Detailed Setup
    3. 2.3 Circuitry
      1. 2.3.1 Current Sensing IC
      2. 2.3.2 Input Signal Path
      3. 2.3.3 Digital Circuitry
    4. 2.4 PAMB Compatibility
  8. 3Software
    1. 3.1 Setup
      1. 3.1.1 Driver Installation
      2. 3.1.2 Firmware
        1. 3.1.2.1 Firmware Debug
      3. 3.1.3 GUI Setup and Connection
        1. 3.1.3.1 Initial Setup
        2. 3.1.3.2 GUI to EVM Connection
    2. 3.2 GUI Operation
      1. 3.2.1 Homepage Tab
      2. 3.2.2 Configuration Tab
      3. 3.2.3 Registers Tab
      4. 3.2.4 Results Data Tab
    3. 3.3 Direct EVM USB Communication
      1. 3.3.1 Standard USB Read and Write Operations
      2. 3.3.2 Collect Data Through the USB BULK Channel
  9. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layout
    3. 4.3 Bill of Materials
  10. 5Additional Information
    1. 5.1 Trademarks
  11. 6Related Documentation

Registers Tab

To view and edit the device registers, click the INA2227EVM (Registers) icon on the menu to the left. The Registers tab looks similar to the one shown in Figure 3-9.

INA2227EVM GUI Registers TabFigure 3-9 GUI Registers Tab

From this page, the user can read and write device registers on the EVM. Here are some important notes:

  • Use the Selected EVM drop-down menu at the top to choose which device to work with on the Registers tab.
    • Note, changing this here also changes the same setting for the Configuration tab.
    • Functionally, this button sets the default read/write address in the MCU and then reads all register values back to update the register map. Note that if data is currently collecting at a high frequency, then this can cause a minor delay in the data collection. To prevent this, set the device settings before starting data collection.
  • By default, all changes are automatically written to the device. If desired, then the user can change the Immediate Write setting to Deferred Write to only allow writing when ready.
    • Users can modify writable register values from any of these methods:
      • Through the widget settings in the Field View section on the right.
      • Changing the Value directly with either hex or decimal values.
      • Double-clicking on any individual bit.
  • Turning on Auto Read only updates registers in the Registers tab, and not the plots in the Results Data section.
    • Leaving Auto Read on while collecting data for plots can interfere with data collection timing.
  • For questions about a register or register bit field, click the INA2227EVM icon.
    • For even more questions about registers, check the data sheet.
  • For convenience, register settings can be saved and loaded back later to any device with the same register map. To do this, go to File > Register Data, as shown in Figure 3-10.
    INA2227EVM Save and Load Register SettingsFigure 3-10 Save and Load Register Settings
    • Press the Read All Registers button after loading data to update the Registers tab with the actual device values, in case the loaded registers are not compatible with the connected device.