To begin the design process, determine
the following:
- Input voltage range
- Use the supply voltage of the device that is driving the TXG404x-Q1 device to determine the input
voltage range. For a valid logic-high, the value must exceed the
positive-going input-threshold voltage (VT+) of the input
port. For a valid logic low the value must be less than the
negative-going input-threshold voltage (VT-) of the input
port.
- Output voltage range
- Use the supply voltage of the device that the TXG404x-Q1 device is driving to determine the output voltage
range.