SCEU033 July 2025
PRODUCTION DATA
The TPLD2001 has an optional I2C address hardware configuration feature that allows the TPLD2001's I2C address to be set via the state of certain pins on device start-up. This block contains pull-up and pull-down resistors that can used to set the I2C address of the TPLD2001. To set the device's I2C address, use shunts to set each bit of the address as either 1 or 0. To set a bit as 1, place a shunt between the middle pin of the address bit and the pin labeled 1. To set a bit as 0, place a shunt between the middle pin of the address bit and the pin labeled 0.
| I2C Address Bit | Pin Number | IO Name |
|---|---|---|
| 0 | 7 | IO5 |
1 | 6 | IO4 |
2 | 5 | IO3 |
3 | 4 | IO2 |