SCEU033 July 2025
PRODUCTION DATA
The programmer header block accepts the 14-position cable used to connect the TPLD2001-RJY-EVM to the TPLD-PROGRAM. TI recommends using this header to connect only to the TPLD-PROGRAM using the cables included in the TPLD-PROGRAM kit. The header is keyed, so the 14-position cable can only be inserted to the case with the key facing the correct direction. To connect the TPLD2001-RJY-EVM to a TPLD-PROGRAM, follow the steps in Section 3.2.
SW3 connects the 3V3 line of the programmer header to the VCC line of the EVM. When powering the EVM from the TPLD-PROGRAM, the 3V3 line must be in the ON position.