SCEU034 July 2025
PRODUCTION DATA
Each LED block consists of an LED that can be connected or disconnected from the TPLD pin via a header. To connect the LED to the corresponding pin, place a shunt on the corresponding header between the two header pins.
Figure 2-5 LED Blocks