SDAA071 September   2025 AM62L

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Using the Power Estimation Tool
    1. 2.1 Processor Cores
    2. 2.2 LVCMOS IO
    3. 2.3 Peripherals
    4. 2.4 Estimated Power Consumption
  6. 3Example Use Case
  7. 4Summary
  8. 5References

Using the Power Estimation Tool

The PET Summary tab allow users to represent the use case by entering the frequency and utilization for all COREs as well as the configuration and utilization for peripherals and IOs. The following sections explain the process in more details.

Note: This Power Estimation Tool does not support the enable or disable of power domains or LPSC. All power domains are enabled by default. Similarly, PLLs and HSDIVs are not modifiable fields with the except of Main PLL8_HSDIV0 which is assigned to the A53s and can be modified in the PET.