SDAA071 September 2025 AM62L
This section shows an example to help users validate the AM62L power estimation tool before entering a specific use case. This example represents a generic HMI use case that uses the parallel display (DSS-DPI), 2xA53 (approximately 80% utilization, 1250MHz) and CPSW at strong process corner, nominal voltage and high temperature. If the calculated power differs from the numbers shown in Figure 3-1, then TI recommends to check the Excel system separators under advanced settings. For proper operation, this spreadsheet uses "." as the decimal separator and "," as the thousands separator.