SDAA115 November   2025 INA190

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Simulation and Best Layout Practices
  6. 3Results
  7. 4Summary
  8. 5Supplementary
  9. 6References

Results

To test the PCB layouts, first the Device Under Test (DUT) was connected to a DC supply (Xantrex XHR 7.5-80), electronic load (Kikusui PLZ1205W) and a precision resistor as shown below in Figure 3-1. The shunts used in bench test were all 300µΩ, hence Reffective is calculated to be 100µΩ. TL-BR spade connector combination was used to flow current through the DUT.

 Bench Test Setup SchematicFigure 3-1 Bench Test Setup Schematic

The precision resistor of 0.01Ω used in the bench test was to accurately determine the load current flowing in the circuit. A Keysight 3458A digital multimeter was used here to determine voltage drop across the precision resistor (Vshunt), then this value is divided by the resistance (0.01Ω) to calculate the load current (Iload Real). Another Keysight 3458A was connected across the OUT pin of DUT and ground to measure Vout.

The results are listed in Table 3-1 and the Error% against load current is plotted in Figure 3-2.

Error % = ((| Expected Vout - Measured Vout |) / Expected Vout) × 100
Table 3-1 Bench Test Results
Layout 1Layout 2Layout 3Expected
Iload (A)DUT Vout (V)Vshunt (mV)Iload Real (A)DUT Vout (V)Vshunt (mV)Iload Real (A)DUT Vout (V)Vshunt (mV)Iload Real (A)DUT Vout (V)
50.104287950.039295.0039290.08969750.023685.0039660.101351750.039665.0023680.100
100.2095919100.009510.000950.180312100.034910.0049280.2036846100.0492810.003490.200
150.3148474150.067815.006780.27096150.054615.00680.3061003150.06815.005460.300
200.4200059200.093520.009350.361594200.080720.009130.4085625200.091320.008070.400
 Layout Comparison PlotFigure 3-2 Layout Comparison Plot