SDAA129 September   2025 TCAN2410-Q1 , TCAN2411-Q1 , TCAN2450-Q1 , TCAN2451-Q1 , TCAN2845-Q1 , TCAN2847-Q1 , TCAN2855-Q1 , TCAN2857-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2What is Channel Expansion
  6. 3What is the GFO Pin and How Does it Apply to Channel Expansion
  7. 4Example Setups of Using GFO Pin in Channel Expansion Based Applications
  8. 5Summary
  9. 6References

Summary

In many applications there can be a need to add an additional transceiver channel for communication, adding another CAN and LIN transceiver to the application. The general design is simple: connect the GFO pin to the proper control input of an external transceiver and use the application software to determine when to turn on the external transceiver. With this knowledge, another design tool has been added to the toolbox of strategies to employ when working with TI SBCs.