SDAA138 September   2025 AM2611 , AM2612 , AM2612-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2USB Host Detection
    1. 2.1 General USB Host Detection Flow
    2. 2.2 AM261x USB Host Detection
  6. 3Hardware Modifications
  7. 4Software Modifications
    1. 4.1 Changes in the USB Synp Driver
    2. 4.2 Changes in the USB Application
    3. 4.3 Steps to Rebuild the USB Driver and Application
      1. 4.3.1 Rebuilding USB Libs
      2. 4.3.2 Rebuilding USB Application
        1. 4.3.2.1 CCS Build
        2. 4.3.2.2 Command Line Build
    4. 4.4 Testing the New Application
  8. 5Summary
  9. 6References

CCS Build

If the application is already in the CCS workplace, right-click on the application and click on Re-build. This rebuilds and relinks the updated USB driver.

 CCS Example Build
                    Steps Figure 4-8 CCS Example Build Steps