SDAA138 September   2025 AM2612

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2USB Host Detection
    1. 2.1 General USB Host Detection Flow
    2. 2.2 AM261x USB Host Detection
  6. 3Hardware Modifications
  7. 4Software Modifications
    1. 4.1 Changes in the USB Synp Driver
    2. 4.2 Changes in the USB Application
    3. 4.3 Steps to Rebuild the USB Driver and Application
      1. 4.3.1 Rebuilding USB Libs
      2. 4.3.2 Rebuilding USB Application
        1. 4.3.2.1 CCS Build
        2. 4.3.2.2 Command Line Build
    4. 4.4 Testing the New Application
  8. 5Summary
  9. 6References

Rebuilding USB Libs

MCU_PLUS_SDK libraries cannot be rebuilt from CCS. Run the following commands to re-build the TINYUSB stack and the USB driver from the MCU_PLUS_SDK directory.

 Rebuilding USB Libraries using
                                                  MakefilesFigure 4-7 Rebuilding USB Libraries using Makefiles