SDAA154 October 2025 AMC0300D , AMC0300D-Q1 , AMC0300R , AMC0300R-Q1 , AMC0306M05 , AMC0306M05-Q1 , AMC0306M25 , AMC0306M25-Q1 , AMC131M03 , AMC131M03-Q1 , AMC3301 , AMC3301-Q1 , AMC3302 , AMC3302-Q1 , AMC3306M05 , AMC3306M05-Q1 , AMC3306M25 , AMC3306M25-Q1
Corresponding to the previous power supply option discussed, the gate driver supply with LDO power supply design also includes a gate driver supply but with an LDO instead of a Zener diode. For similarly low-cost applications where it is crucial to provide stable voltage with low noise to the gate driver, an LDO may be favored to regulate the voltage. LDOs can help stabilize the power in conditions such as expected system voltage spikes or overheating.
LDOs offer better regulation than diodes do. They provide a more stable output voltage with fluctuating load or input current. LDOs are also preferred for applications where the input voltage and output voltage are only a small difference. When designing with an LDO, the additional voltage drop of the LDO needs to be considered too. This involves selecting resistor values to establish the output voltage at the AMC's necessary supply voltage. Including capacitors to counteract reactive input sources and improve transient responses are required steps in this design process with LDOs. As the schematic in Figure 2-3 shows, the isolated gate driver power supply is established after the DC link. This power supply option can be used in rectifier or inverter applications, which is covered later in the app note. Both of these applications include active switches that can benefit from the stable output of a gate driver supply. A gate driver with an LDO further reduces noise from the power supply helping bolster the stability of this power supply suitable for many applications.
The TLV709 is a good LDO option for many applications. This LDO can operate with 2.5V to 30V on the input which makes it preferred for many power supply rails that can source the gate driver. This device also has adjustable outputs, meaning with a simple resistive divider a user can establish the output voltage to be that of the high-side power supply – for example 3.3V or 5V for most AMC devices. This is demonstrated in the AMC-MOD-50A-EVM Evaluation Board. See the Analog Input section of the user's guide for more information.