SDAA265 April 2026 TPS25751A , TPS26750A
Assume there is a system that has the default settings discussed however the following are selected:
This PD device is EPR-capable and can successfully enter into EPR mode with an EPR-capable USB-PD Source. However the PD device only requests 20V even in EPR mode. This is due to the fact that the AUTO_NEGOTIATE_SINK.AutoNegMaxVoltage is configuration (or set by the EC) to 20V meaning the PD device never accepts any voltage higher than 20V.
Figure 5-2 20V PDO Requested in EPR
Mode