SDAA280 March 2026 MSPM0G5187
Another option for power on a USB device can be self-powering. This means that on the device, there is some external power supply apart from the USB power, which provides power to the chip and the connection when necessary.
A typical example of such a mode can be an audio or storage device, where power is required despite being disconnected. These designs require additional power management when compared to the bus-powered mode, with some form of primary power regulator and sequencing depending on the complexity of the power tree.
Oftentimes, self-powered devices can also be considered hybrid, meaning they either use the bus power when connected or charge a battery when connected. For this reason, oftentimes a VBUS monitoring circuit is necessary to detect a connection and switch to the power path provided by the bus. This can be accomplished by something as simple as a resistor divider hooked up to an ADC pin on the MSPM0G5187, which toggles a switch on the power path.