SDAA309 May   2026 OPA2991 , OPA2992 , OPA4991 , OPA4992 , OPA991 , OPA992 , TLV9151 , TLV9152 , TLV9154 , TLV9161 , TLV9162 , TLV9164 , TLV9351 , TLV9352 , TLV9354 , TLV9361 , TLV9362 , TLV9364

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Full Power Bandwidth Theory
  6. 3 Understanding Slew Rate
  7. 4 Understanding Slew Boost
  8. 5 Measuring THD Limited Full Power Bandwidth
  9. 6 Interpreting the Full Power Bandwidth Curves
  10. 7 Impact of Slew Boost Architecture on Full Power Bandwidth Model
  11. 8 THD Limited Full Power Bandwidth Dependence on Closed Loop & Open Loop Gain
  12. 9 Summary
  13. 10Appendix
  14. 11References

Understanding Slew Rate

Figure 3-1 shows a simplified block diagram of an operation amplifier. The first stage is a transconductance (gm) stage that converts the input differential voltage (Vid) into a current, IM, known as the Miller Current. This current flows into the Miller capacitance (CM) of the transimpedance stage where the current IM is converted to a voltage at the output node Vout.

 Op amp internal block
                    diagram Figure 3-1 Op amp internal block diagram

Figure 3-2 shows the transfer function for an op amp transconductance stage. The small signal response is shown in green and the large signal step response (slew rate limit) is shown in blue.

 Transfer function for op amp
                    transconductance stage Figure 3-2 Transfer function for op amp transconductance stage

Small signal operation- Small signal operation can be defined as when Vid is modest (for example Vid < 100mV, see Figure 3-2), and the transconductance stage behaves linearly. Equation 2 describes the small signal relationship between the miller current and input differential voltage.

Equation 2. I M = g m Ă— V i d

During small signal operation, the current IM is directly proportional to Vid. In a closed loop configuration the output voltage is fed back to the inputs with an external feedback network. The feedback forces the voltage difference (Vid) between the inverting and non-inverting inputs toward zero. Although the inverting and non‑inverting terminals are not electrically connected, the high open loop gain (AOL) of the op amp forces the voltage difference between them to be extremely small; an effect commonly referred to as a virtual short. For example, a 1mV step applied to the inputs generates a brief current pulse into CM, which makes the output rise. As the Miller capacitor charges, the feedback forces the input differential voltage towards the "virtual short" condition, and when the transient settles Vid is essentially zero.

Large signal (slew rate limited) operation- If the input differential voltage exceeds the linear range (for example Vid > 100mV, see Figure 3-2), the transconductance stage produces the peak current IM_Max that charges the miller capacitor CM as shown in Figure 3-3. This constant current continues to charge CM, producing a linear ramp at the output node Vout:

Equation 3. SR = dVOUT dt = I M_Max C M

The resulting slope of the output voltage ramp defines the slew rate; the maximum rate which the op amp output can change. With a large step applied, the output initially follows this slew rate limit while the feedback simultaneously reduces the input differential voltage. Once the input differential voltage falls back into the small signal region of operation, IM falls exponentially towards zero and the output transition changes from a linear ramp to an exponential settling curve. The differential input finally reaches the virtual short condition. Figure 3-3 provides a magnified view of the waveforms, highlighting the moment the device enters small signal mode of operation and illustrates how the input differential voltage decays exponentially toward 0V.

 Vid and
                        IM for a large signal step Figure 3-3 Vid and IM for a large signal step