SDAA309 May   2026 OPA2991 , OPA2992 , OPA4991 , OPA4992 , OPA991 , OPA992 , TLV9151 , TLV9152 , TLV9154 , TLV9161 , TLV9162 , TLV9164 , TLV9351 , TLV9352 , TLV9354 , TLV9361 , TLV9362 , TLV9364

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Full Power Bandwidth Theory
  6. 3 Understanding Slew Rate
  7. 4 Understanding Slew Boost
  8. 5 Measuring THD Limited Full Power Bandwidth
  9. 6 Interpreting the Full Power Bandwidth Curves
  10. 7 Impact of Slew Boost Architecture on Full Power Bandwidth Model
  11. 8 THD Limited Full Power Bandwidth Dependence on Closed Loop & Open Loop Gain
  12. 9 Summary
  13. 10Appendix
  14. 11References

THD Limited Full Power Bandwidth Dependence on Closed Loop & Open Loop Gain

The mechanisms discussed in this section are distinct from the significant slew induced waveform distortion described earlier. This section instead focuses on how feedback and loop gain influence small signal linearity and harmonic distortion. A fundamentally important point to establish in this section is that the reduction in loop gain with increasing closed loop gain does not directly change the classical slew rate limit full power bandwidth curve for a fixed amplitude.

Figure 8-1 shows the measured full power bandwidth curves for the OPA991 in three different closed loop gain configurations; ACL = 1 V V , 11 V V and 101 V V . Each curve represents a fixed distortion limit of THD = -60dB. The measured full power bandwidth curves show a clear dependency on closed loop gain, with higher gains exhibiting reduced bandwidth, f FPBW ( A CL = 101 V V ) < f FPBW ( A CL = 11 V V ) < f FPBW ( A CL = 1 V V ) . The classic full power bandwidth model, which assumes a single well defined slew rate limit and also ignores the impact of closed loop gain, does not predict this behavior.

 OPA991 Full Power Bandwidth
                    (THD = -60dB) at Three Different Signal Gains Figure 8-1 OPA991 Full Power Bandwidth (THD = -60dB) at Three Different Signal Gains

Analyzing the feedback equations of an operational amplifier helps explain why increasing the closed loop gain (ACL) reduces the THD defined full power bandwidth curve.

Figure 8-2 shows the block diagram for an operational amplifier in a closed loop configuration.

 Feedback Control Theory Block
                    Diagram Figure 8-2 Feedback Control Theory Block Diagram

Recall that the closed loop gain equation for an operational amplifier is:

Equation 6. A C L ( f ) = V o u t ( f ) V i n ( f ) = A O L ( f ) 1 + A O L ( f ) β ( f ) ≈ 1 β ( f ) , A O L ( f ) · β ( f ) ≫ 1

Where:

AOL(f) open loop gain
β(f) external feedback factor
AOL(f)β(f) Loop Gain
For further details on the derivation of this equation please visit the Texas Instruments Precision Labs Series.

Rewriting Equation 6 and solving for β results in Equation 7.

Equation 7. β ( f ) = A OL ( f ) − A CL ( f ) A OL ( f ) ⋅ A CL ( f )

One observation to make when analyzing Equation 7 is that higher ACL results in a reduced β since these parameters are inversely proportional. This in turn lowers the loop gain AOLβ. The loop gain is the parameter that controls the error voltage Vid between the op amp inputs. Since loop gain directly controls the input error voltage (Vid), understanding the relationship between Vid and loop gain is crucial.

To start, rewriting Equation 6 and solving for Vout results in:

Equation 8. V o u t ( f ) = V i n ( f ) A O L ( f ) 1 + A O L ( f ) β ( f )

As seen in Figure 8-2:

Equation 9. V i d ( f ) = V o u t ( f ) A O L ( f )

Substituting Equation 8 into Equation 9 results in:

Equation 10. V i d ( f ) = V i n ( f ) 1 + A O L ( f ) β ( f )

The inverse relationship between Vid and AOLβ shown in Equation 10 demonstrates that a reduction in loop gain results in an increase in the error voltage Vid at the inputs of the op amp. Because loop gain is the mechanism that linearizes the amplifier transfer function, a lower loop gain diminishes the ability of the system to correct internal nonlinearities. This increase in error voltage results in greater signal distortion and higher THD. As THD increases, the measured bandwidth of the THD defined full power bandwidth curve is reduced. In summary, the relationship between higher ACL and reduced THD defined full power bandwidth performance follows this progression:

A C L ↑ ⇒ β ↓ ⇒ Loop Gain ↓ ⇒ V i d  Nonlinearity ↑ ⇒ THD ↑ ⇒ Measured THD Defined f FPBW ↓

Loop gain is also dependent on the op amp open loop gain AOL, which is finite and rolls off with frequency. Consequently, as AOL declines, loop gain decreases and as a result the total harmonic distortion (THD) increases.

The reduction in loop gain with increasing closed loop gain does not directly change the slew rate limit full power bandwidth boundary of the amplifier. Instead, reduced loop gain increases the input error voltage Vid, which increases small signal nonlinear distortion and raises THD prior to the onset of significant visual slew induced waveform collapse. As a result, the THD defined full power bandwidth curve contracts with increasing closed loop gain even though the underlying slew rate limit full power bandwidth boundary of the amplifier remains unchanged.

More information on THD can be found in How to Measure Total Harmonic Distortion of an Op-Amp and THD + N Fundamentals and the Texas Instruments Precision Labs video series on op amp distortion.