SDAA333 June   2026 TXB0604 , TXB0606

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2How Does the TXB0604 Compare to Legacy and Existing Market Solutions?
    1. 2.1 Recommended Device Selection
  6. 3Case Study
    1. 3.1 Performance with Light Capacitive Loads
    2. 3.2 Performance with Heavy Capacitive Loads
    3. 3.3 Performance with Distributed Capacitive Loads
  7. 4Design Considerations with the TXB0604/ TXB0606
    1. 4.1 Impedance Matching
    2. 4.2 Direction Change Wait Time, TDCW
  8. 5Summary
  9. 6References

Introduction

This app note is an extension of Overcoming TXB-Type Translators Design Challenges, and addresses design challenges specific to the TXB‑type translators (TXB010x, TXB030x, TXB060x). While all three devices resolve mismatched operating voltages for bidirectional data signals, the TXB0604/ TXB0606 is unique in that the device also helps designers mitigate noise and bandwidth limitations caused by transmission‑line effects. In this application note, the capabilities of the TXB0604 and TXB0606 is demonstrated through a bench setup of the 4-channel equivalent, accompanied by waveforms from the leading devices of today. This industry‑leading design enables designers to achieve higher throughput even when faced with moderate to severe capacitive‑load buses, conditions that were previously thought not preferred for legacy or competitive designs. For the background use case of the TXB0604/ TXB0606 and examples of where it can be applied, see From Bottleneck to Breakthrough: QSPI Optimization in Data Centers with TXB0604/TXB0606.

For a list of recommended level‑translation devices for common interface types, visit TI’s Voltage Translators and Level Shifters page.