SDAA445A August 2026 – August 2026 HDC1010 , HDC1080 , HDC2010 , HDC2021 , HDC2022 , HDC2080 , HDC3020 , HDC3020-Q1 , HDC3021 , HDC3021-Q1 , HDC3022 , HDC3022-Q1 , HDC3120 , HDC3120-Q1
In Figure 2-3, a more polar molecule is contaminating the sensing polymer. Because the overall dielectric constant is being changed from what just water vapor would do, the RH output changes as well. In this case, negative RH gain and positive RH error shifts can be expected. Water vapor has a very high dielectric constant, as seen in Figure 2-3, even compared to other chemical contaminants. This means that when ambient RH is high, the RH sensor output will shift down since less of the highly polar water vapor molecules can penetrate the polymer due to the presence of the contaminant. Conversely, at lower ambient RH levels the RH output is elevated because the polar molecules are increasing the overall dielectric constant of the polymer.