SDAA445A August   2026  – August 2026 HDC1010 , HDC1080 , HDC2010 , HDC2021 , HDC2022 , HDC2080 , HDC3020 , HDC3020-Q1 , HDC3021 , HDC3021-Q1 , HDC3022 , HDC3022-Q1 , HDC3120 , HDC3120-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Why Chemical Contamination Occurs
    2. 1.2 Types and Sources of Chemical Contaminants
  5. 2Detailed Description
    1. 2.1 Mechanism of Containment Interaction With Sensors
    2. 2.2 Non-Polar Chemical Contamination
    3. 2.3 Polar Chemical Contaminations
    4. 2.4 Ionic Chemical Contamination
    5. 2.5 Surface Chemical Contamination
    6. 2.6 What Preventative Actions Can Be Taken?
  6. 3Summary
  7. 4References
  8. 5Revision History

Non-Polar Chemical Contamination

Non-polar solvents in low concentrations have minimal to no interaction with functional groups of the polymer when exposed in limited quantities. Thus, chemicals such as cyclopentane or Toluene have negligible impact on sensor accuracy. This is shown in Figure 2-2. Non-polar molecules do not penetrate deep into the polymer matrix and have a relatively small impact on RH output. Since the non-polar molecules are still taking the place of water vapor molecules in the polymer voids, they do slightly reduce the RH output.

 Small Shift in RH Accuracy
                    from Non-Polar Contamination Figure 2-2 Small Shift in RH Accuracy from Non-Polar Contamination