SDAA450 July   2026 AM2431 , AM2432 , AM2434 , AM2752-Q1 , AM2754-Q1 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Mechanism of ENET FOTA
  6. 3 Ethernet Setup
    1. 3.1 Linux System
    2. 3.2 Windows System
  7. 4 Authenticated FOTA
    1. 4.1 Signing the Firmware
  8. 5 Encrypted FOTA
    1. 5.1 Signing and Encrypting the Firmware
  9. 6 Software Structure
    1. 6.1 AM243x/AM64x
    2. 6.2 AM275x
  10. 7 Expected Outputs
    1. 7.1 AM243x/AM64x
    2. 7.2 AM275x
  11. 8 Performance Metrics
  12. 9 Summary
  13. 10References

Linux System

  • Connect the Ethernet cable between the Host and the EVM.
  • Assign an IP Address having the same subnet as the EVM, using the following command:
sudo ifconfig <interface-name> <Host IP Address> <Subnet mask>
  1. example:sudo ifconfig eno1 192.168.0.193 netmask 255.255.255.0
  2. Run the ip link or ifconfig command to find the name of your network interface.
  • Add a static ARP entry with the command below:
sudo arp -i <interface-name> -s <IP Address of EVM> <MAC-Address of EVM>
  1. example: sudo arp -i eno1 -s 192.168.0.195 44:6b:1f:2c:2d:25