SDAA526 September 2026 THVD4431A
Because the transient occurs only during the DIR transition period when the receiver is being enabled, the UART of the MCU is typically not actively sampling. If the transient is captured by the UART, firmware can be configured to ignore the RX signal during the direction-change window as a temporary workaround.