SFFSAY6 December   2025 ISOTMP35R-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
  7. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the ISOTMP35R-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the ISOTMP35R-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the ISOTMP35R-Q1 data sheet.

ISOTMP35 Pin Diagram Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • A bypass capacitor of 0.1μF on the input voltage pin is implemented.
  • The capacitive loading on the output pin is limited to 220nF.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VDD 1 The device is not powered. The device is not functional. Observe that the absolute maximum ratings for all pins of the device are met; otherwise, device damage is plausible. A
NC 2 There is no effect on the device. The device operates as normal. D
VOUT 3 The output is stuck low. There is no analog output present on the device. B
NC 4 There is no effect on the device. The device operates as normal. D
GND 5 There is no effect on the device. The device operates as normal. D
NC 6 There is no effect on the device. The device operates as normal. D
TSENSE 7 There is no effect on the device. The device operates as normal. D
TSENSE 8 There is no effect on the device. The device operates as normal. D
TSENSE 9 There is no effect on the device. The device operates as normal. D
TSENSE 10 There is no effect on the device. The device operates as normal. D
TSENSE 11 There is no effect on the device. The device operates as normal. D
TSENSE 12 There is no effect on the device. The device operates as normal. D
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VDD 1 The functionality of the device is undetermined. B
NC 2 There is no effect on the device. The device operates as normal. D
VOUT 3 There is no effect on the device. The device operates as normal. D
NC 4 There is no effect on the device. The device operates as normal. D
GND 5 The functionality of the device is undetermined. The device is not powered or internally connected to ground through an ESD diode of an alternate pin and powers up. B
NC 6 There is no effect on the device. The device operates as normal. D
TSENSE 7 There is no effect on the device. The device operates as normal. D
TSENSE 8 There is no effect on the device. The device operates as normal. D
TSENSE 9 There is no effect on the device. The device operates as normal. D
TSENSE 10 There is no effect on the device. The device operates as normal. D
TSENSE 11 There is no effect on the device. The device operates as normal. D
TSENSE 12 There is no effect on the device. The device operates as normal. D
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
VDD 1 NC There is no effect on the device. The device operates as normal. D
NC 2 VOUT There is no effect on the device. The device operates as normal. D
VOUT 3 NC There is no effect on the device. The device operates as normal. D
NC 4 GND There is no effect on the device. The device operates as normal. D
GND 5 NC There is no effect on the device. The device operates as normal. D
TSENSE 7 TSENSE There is no effect on the device. The device operates as normal. D
TSENSE 8 TSENSE There is no effect on the device. The device operates as normal. D
TSENSE 9 TSENSE There is no effect on the device. The device operates as normal. D
TSENSE 10 TSENSE There is no effect on the device. The device operates as normal. D
TSENSE 11 TSENSE There is no effect on the device. The device operates as normal. D
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VDD 1 There is no effect on the device. The device operates as normal. D
NC 2 There is no effect on the device. The device operates as normal. D
VOUT 3 The output is stuck high. B
NC 4 There is no effect on the device. The device operates as normal. D
GND 5 The functionality of the device is undetermined. Observe that the absolute maximum ratings for all pins of the device are met; otherwise, device damage is plausible. A
NC 6 There is no effect on the device. The device operates as normal. D
TSENSE 7 There is no effect on the device. The device operates as normal. D
TSENSE 8 There is no effect on the device. The device operates as normal. D
TSENSE 9 There is no effect on the device. The device operates as normal. D
TSENSE 10 There is no effect on the device. The device operates as normal. D
TSENSE 11 There is no effect on the device. The device operates as normal. D
TSENSE 12 There is no effect on the device. The device operates as normal. D