SFFSBP6 November 2026 TPS281C100
This section provides a failure mode analysis (FMA) for the pins of the TPS281C100x. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality. |
| B | No device damage, but loss of functionality. |
| C | No device damage, but performance degradation. |
| D | No device damage, no impact to functionality or performance. |
Figure 4-1 shows the TPS281C100x pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPS281C100x datasheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| OL_ON | 1 | High accuracy sense mode is disabled. | C |
| SNS | 2 | The sense current is not valid from the SNS pin. | B |
| ILIM | 3 | The device defaults to the internal current limit. | C |
| NC | 4, 9 | There is no effect on the device. | D |
| VOUT | 5, 6 | The current limit of the device engages. | B |
| VS | 7, 8 | The device has no input supply, and therefore, does not function. | B |
| FAULT | 10 | The reported status can be erroneous. | B |
| DIAG_EN | 11 | The diagnostics disable. | B |
| EN | 12 | The output shuts down. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| OL_ON | 1 | High accuracy sense mode disables. The OL_ON pin pulls down internally. | B |
| SNS | 2 | The correct sense current cannot be read. | B |
| ILIM | 3 | The device defaults to the internal current limit. | C |
| NC | 4, 9 | There is no effect on the device. | D |
| VOUT | 5, 6 | There is no effect on the device. The open load detection triggers. | B |
| VS | 7, 8 | The device has no input supply, and therefore, does not function. | B |
| FAULT | 10 | The fault signal is not reported. | B |
| DIAG_EN | 11 | The pin is internally pulled down. The diagnostics disable. | B |
| EN | 12 | The output shuts down and the EN pin pulls down internally. | B |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| OL_ON | 1 | SNS | The current sensing output is erroneous. The device is in standard sensing or high accuracy sensing depending on the output of the SNS pin. | B |
| SNS | 2 | ILIM | The current limit and current sensing outputs are incorrect. | B |
| ILIM | 3 | NC | There is no effect on the device. | D |
| NC | 4 | VOUT | There is no effect on the device. | D |
| VS | 8 | NC | There is no effect on the device. | D |
| NC | 9 | FAULT | There is no effect on the device. | D |
| FAULT | 10 | DIAG_EN | Fault reporting is erroneous. Diagnostics enable if FAULT pulls high. | B |
| DIAG_EN | 11 | EN | The EN signal effects the DIAG_EN signal and vice versa. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| OL_ON | 1 | There is a potential violation of the absolute maximum rating of the pin and a possible breakdown of the ESD cell. | A |
| SNS | 2 | There is a potential violation of the absolute maximum rating of the pin and a possible breakdown of the ESD cell. | A |
| ILIM | 3 | There is a potential violation of the absolute maximum rating of the pin and a possible breakdown of the ESD cell. | A |
| NC | 4, 9 | There is no effect on the device. | D |
| VOUT | 5, 6 | The output pulls to supply voltage. | B |
| FAULT | 10 | There is a potential violation of the absolute maximum rating of the pin and a possible breakdown of the ESD cell. | A |
| DIAG_EN | 11 | There is a potential violation of the absolute maximum rating of the pin and a possible breakdown of the ESD cell. | A |
| EN | 12 | There is a potential violation of the absolute maximum rating of the pin and a possible breakdown of the ESD cell. | A |