SGLS247C September 2011 – December 2025 TPS763-Q1
PRODUCTION DATA
The EN pin for the device is an active-high pin. The output voltage is enabled when the voltage of the EN pin is greater than the high-level input voltage of the EN pin and disabled with the EN pin voltage is less than the low-level input voltage of the EN pin. If independent control of the output voltage is not needed, connect the EN pin to the input of the device.
The device has an internal pulldown circuit that activates when the device is disabled by pulling the EN pin voltage lower than the low-level input voltage of the EN pin to actively discharge the output voltage.