SLAA913A January 2020 – June 2021
In this test both the sensor readout (HDC readout in automatic mode) and the RF packet transmit period are set to once per minute. The RF parameters are the default settings for 50 kbps, 2-GFSK in SmartRF Studio at +1 dBm. All these parameters are equal to the settings of the TIDA-00484 reference design to enable comparison between the different system solutions. Figure 4-1 shows the current profile, captured by the EnergyTrace function in CCS with a total transmit time of nearly 6.2 ms. The last 2.5 ms of this pulse with a stable current of approximately 9.4 mA shows the wireless data transmission by the CC1352P device (note that EnergyTrace reports relative measurement values, the CC1352P data sheet value is 9 mA).
Figure 4-1 Current Profile for +1-dBm Transmit With SCE and
Arm®Cortex®-M4F Activity