SLAAE70A December 2022 – February 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
The BSL is a program that is stored in the MSPM0 flash or ROM at the factory. The BSL is used for programming, erasing, and reading code stored in main memory, information memory, or RAM. The BSL communication interface and reset pins are used when updating the code using the BSL. For more details about the BSL and its communication interface, see the bootstrap loader (BSL) section in the device-specific data sheet.