SLAAEJ3A January   2024  – August 2025 MSPM0G1106 , MSPM0G1107 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1

 

  1.   1
  2.   2
  3. 1Revision History
  4.   Trademarks

Design Description

This subsystem demonstrates how to build a CAN-SPI bridge. CAN-SPI bridge allows a device to send or receive information on one interface and receive or send the information on the other interface Download the code for this example. The subsystem supports SPI to work in controller mode or peripheral mode.

Figure 1-1 shows a functional diagram of this subsystem.

 Subsystem Functional Block
                    Diagram Figure 1-1 Subsystem Functional Block Diagram

Required Peripherals

This application requires CANFD and SPI.

Table 1-1 Required Peripherals
Sub-block Functionality Peripheral Use Notes
CAN interface (1x) CANFD Called MCAN0_INST in code
SPI interface (1x) SPI Called SPI_0_INST in code

Design Steps

  1. Determine the basic setting of CAN interface, including CAN mode, bit timing, message RAM configuation and so on. Consider which setting is fixed and which setting is changed in the application. In example code, CANFD is used with 250kbit/s arbitration rate and 2Mbit/s data rate.
    1. Key features of the CAN-FD peripheral include:
      1. Dedicated 1KB message SRAM with ECC
      2. Configurable transmit FIFO, transmit queue and event FIFO (up to 32 elements)
      3. Up to 32 dedicated transmit buffers and 64 dedicated receive buffers. Two configurable receive FIFOs (up to 64 elements each)
      4. Up to 128 filter elements
    2. If CANFD mode is enabled:
      1. Full support for 64-byte CAN-FD frames
      2. Up to 8Mbit/s bit rate
    3. If CANFD mode is disabled:
      1. Full support for 8-byte classical CAN frames
      2. Up to 1Mbit/s bit rate
  2. Determine the CAN frame, including data length, bit rate switching, identifier, data and so on. Consider which part is fixed and which part need to be changed in the application. In example code, identifier, data length and data can change in different frames, while others are fixed. Note that users need to modify the code if protocol communication is required.

    /**
     *  @brief  Structure for MCAN Rx Buffer element.
     */
    typedef struct {
        /*! Identifier */
        uint32_t id;
        /*! Remote Transmission Request
         *   0 = Received frame is a data frame
         *   1 = Received frame is a remote frame
         */
        uint32_t rtr;
        /*! Extended Identifier
         *   0 = 11-bit standard identifier
         *   1 = 29-bit extended identifier
         */
        uint32_t xtd;
        /*! Error State Indicator
         *   0 = Transmitting node is error active
         *   1 = Transmitting node is error passive
         */
        uint32_t esi;
        /*! Rx Timestamp */
        uint32_t rxts;
        /*! Data Length Code
         *   0-8  = CAN + CAN FD: received frame has 0-8 data bytes
         *   9-15 = CAN: received frame has 8 data bytes
         *   9-15 = CAN FD: received frame has 12/16/20/24/32/48/64 data bytes
         */
        uint32_t dlc;
        /*! Bit Rat Switching
         *   0 = Frame received without bit rate switching
         *   1 = Frame received with bit rate switching
         */
        uint32_t brs;
        /*! FD Format
         *   0 = Standard frame format
         *   1 = CAN FD frame format (new DLC-coding and CRC)
         */
        uint32_t fdf;
        /*! Filter Index */
        uint32_t fidx;
        /*! Accepted Non-matching Frame
         *   0 = Received frame matching filter index FIDX
         *   1 = Received frame did not match any Rx filter element
         */
        uint32_t anmf;
        /*! Data bytes.
         *   Only first dlc number of bytes are valid.
         */
        uint16_t data[DL_MCAN_MAX_PAYLOAD_BYTES];
    } DL_MCAN_RxBufElement;

  3. Determine the basic setting of SPI interface, including SPI mode, bit rate, frame size, FIFO, and so on. Consider which setting is fixed and which setting is changed in the application. In example code, SPI can be set as controller or peripheral. SPI operates at 500k bit rate in controller mode.
    1. Key features of the SPI include:
      1. Configurable as a controller or a peripheral
      2. Programmable clock bit rate and prescaler
      3. Separate transmit (TX) and receive (RX) first-in first-out buffers (FIFOs);
      4. Supports PACKEN feature and single bit parity
      5. Programmable data frame size and programmable SPI mode
      6. Interrupts for transmit and receive FIFOs, overrun and timeout interrupts, and DMA done
  4. Determine the SPI frame. Typically SPI is transmitted in bytes. To achieve high-level communication, users can implement frame communication through software. If necessary, users can also introduce specific communication protocols. In example code, the message format is < 55 AA ID1 ID2 ID3 ID4 Length Data1 Data2 ...>. Users can send data to the CAN bus from the terminal by entering data as the same format. 55 AA is the header. ID area is 4 bytes. Length area is 1 byte, indicating the data length. Note that if users need to modify the SPI frame, the code for frame acquisition and parsing also need to be modified.
    Table 1-2 SPI Frame Form
    Header Address Data Length Data
    0x55 0xAA 4 bytes 1 byte (Data Length) bytes
  5. Determine the bridge structure, including what messages need to be converted, how to convert messages and so on.
    1. Consider whether the bridge is one-way or two-way. Typically each interface has two functions: receiving and sending. Consider whether only some functions need to be included (such as SPI reception and CAN transmission). In example code, CAN-SPI bridge is a two-way structure.
    2. Consider what information to convert and the corresponding carrier(variable, FIFO). In example code, identifier, data and data length are convert from one interface to the other interface. There are two FIFOs defined in code as shown inFigure 1-2.
       Bridge
                                    Structure Figure 1-2 Bridge Structure
  6. (Optionally) Consider priority design, congestion situation, error handling and so on.

Design Considerations

  1. Consider the information flow in the application to determine the information to be received or sent by each interface, the protocols to be followed, and design appropriate information transfer carriers to connect different interfaces.
  2. The recommendation is to test the interface separately first, and then implement the overall bridge function. In addition, consider the handling of abnormal situations, such as communication failure, overload, frame format error, and so on.
  3. The recommendation is to implement interface functions through interrupts to make sure of timely communication. In example code, interface functions are usually implemented in the interrupt, and the transfer of information is completed in the main() function.

Software Flowchart

The following figure shows the code flow diagram for CAN-SPI bridge which explains how the messages received in one interface and sent in the other interface. The CAN-SPI bridge can be divided into four independent tasks: receive from SPI, receive from CAN, transmit through CAN, transmit through SPI. Two FIFOs implement bidirectional message transfer and message caching.

Note that SPI is a communication method that sends and receives at the same time. When the controller initiates sending a byte, the controller expects to receive a byte. In the design of this article, SPI RX interrupt is not only used for SPI receive, but also used to fill the TX data into SPI TX FIFO. If SPI works in controller mode, SPI communication starts immediately after SPI TX FIFO is stored by data. If SPI works in peripheral mode, SPI can wait for the controller to initiate communication after data is stored. In this demo, users can select the mode of SPI.

 Application Software
                    Flowchart Figure 1-3 Application Software Flowchart

Device Configuration

This application makes use of TI System Configuration Tool (SysConfig) graphical interface to generate the configuration code for the CAN and SPI. Using a graphical interface to configure the device peripherals streamlines the application prototyping process.

The user can configure the SPI to be controller or peripheral in the Sysconfig.

The code for what is described in Figure 1-3 can be found in the files from example code as shown in Figure 1-4.

 File Structure Figure 1-4 File Structure

Application Code

The following code snippet shows where to modify the interface function. Functions in table are categorized into different files. Functions for SPI receive and transmit are included in bridge_spi.c and bridge_spi.h. Functions for CAN receive and transmit are included in bridge_can.c and bridge_can.h. Structure of FIFO element is defined in user_define.h.

Users can easily separate functions by file. For example, if only SPI functions are needed, users can reserve bridge_spi.c and bridge_spi.h to call the functions.

See the MSPM0 SDK and DriverLib documentation for the basic configuration of peripherals.

Table 1-3 Functions and Descriptions
Tasks Functions Description Location
SPI receive getSpiRxMsg() Get the received SPI message

bridge_spi.c

bridge_spi.h
processSpiRxMsg() Convert the received SPI message format and store it into gSPI_RX_Element
SPI transmit processSpiTxMsg() Convert the gSPI_TX_Element format to be sent through SPI
sendSpiTxMsg() Send message through SPI
CAN receive getCANRxMsg() Get the received CAN message

bridge_can.c

bridge_can.h

processCANRxMsg() Convert the received CAN message format and store the message into gCAN_RX_Element
CAN transmit processCANTxMsg() Convert the gCAN_TX_Element format to be sent through CAN
sendCANTxMsg() Send message through CAN

Custom_Element is the structure defined in user_define.h. Custom_Element is used as the structure of FIFO element, output element of SPI/CAN transmit and input element of SPI/CAN receive. Users can modify the structure according to the need.

typedef struct {
    /*! Identifier */
    uint32_t id;
    /*! Data Length Code*/
    uint32_t dlc;
    /*! Data bytes*/
    uint16_t data[64];
} Custom_Element;

For FIFO, there are 2 global variables used as FIFO. 6 global variables are used to trace the FIFO.

Custom_Element S2C_FIFO[S2C_FIFO_SIZE];
Custom_Element C2S_FIFO[C2S_FIFO_SIZE];
uint16_t S2C_in = 0;
uint16_t S2C_out = 0;
uint16_t S2C_count = 0;
uint16_t C2S_in = 0;
uint16_t C2S_out = 0;
uint16_t C2S_count = 0;

Results

By using CAN analyzer, users can send and receive messages on the CAN side. As a demonstration, two launchpads can be used as two CAN-SPI bridges(one SPI controller and one SPI peripheral) to form a loop. When the CAN analyzer sends CAN messages through controller launchpad, it will receive CAN messages from the peripheral launchpad.

 Demonstration Figure 1-5 Demonstration
 Messages Sent and Received by
                    CAN Analyzer for the Demo Figure 1-6 Messages Sent and Received by CAN Analyzer for the Demo
 PC Terminal Program of Logic
                    Analyzer Figure 1-7 PC Terminal Program of Logic Analyzer

Additional Resources