SLAAEL7A June 2024 – November 2026 TAS2572
Figure 3-1 represents the block diagram representation of the Advanced Battery Guard algorithm. The ABG algorithm regulates the output current drawn from the battery by limiting the output power to the speaker. The current regulation is based on:
With the regulation of the audio based on the aforementioned parameters, the ABG algorithm provides increased loudness and dynamic range on the output audio. At the same time, the algorithm also regulates the output power to avoid clipping on the speaker that is being driven, while keeping the battery above the brownout voltage. The VBAT profile with and without ABG algorithm enabled is compared in Figure 3-1.
The next sections describe the features of the ABG algorithm, and the results were tested using the TAS257x Stereo EVM, with a 1S Lithium-Polymer battery at 10% charge (around 3.6V), and the input audio used being a 1FFS sinusoidal tone at frequencies ranging from 100Hz to 20kHz. The setup is represented in Figure 3-3, and the test signal in Figure 3-4.