SLASFL9A November 2025 – December 2025 MSPM0G5115 , MSPM0G5116 , MSPM0G5117
PRODMIX
The windowed watchdog timer (WWDT) can be used to supervise the operation of the device, specifically code execution. The WWDT can be used to generate a reset or an interrupt if the application software does not successfully reset the watchdog within a specified window of time. Key features of the WWDT include:
For more details, see the WWDT chapter of the MSPM0 G-Series 80-MHz Microcontrollers Technical Reference Manual.