SLAU813A September 2019 – October 2020 TPA6304-Q1
Each channel has the same setting selections: Hi-Z, Mute, Play, Gain, Line Output mode and Speaker mode.
The drop down menu allows the user to select either Hi-Z, Mute or Play Mode for each channel.
The default gain for each channel is 28 dB. The other gain options are 10 dB, 16 dB and 22 dB. If another gain is needed, select the button to the corresponding gain.
The default setting for each channel is Speaker mode. If Line Output is used select the Line Output button.
Figure 4-5 Channel Control Section