SLAZ742H July   2023  – August 2026 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1

 

  1.   1
  2.   Abstract
  3. 1Functional Advisories
  4. 2Preprogrammed Software Advisories
  5. 3Debug Only Advisories
  6. 4Fixed by Compiler Advisories
  7. 5Device Nomenclature
    1. 5.1 Device Symbolization and Revision Identification
  8. 6Advisory Descriptions
    1. 6.1  ADC_ERR_01
    2. 6.2  ADC_ERR_02
    3. 6.3  ADC_ERR_05
    4. 6.4  ADC_ERR_06
    5. 6.5  BSL_ERR_01
    6. 6.6  CLK_ERR_01
    7. 6.7  COMP_ERR_02
    8. 6.8  COMP_ERR_03
    9. 6.9  COMP_ERR_06
    10. 6.10 CPU_ERR_01
    11. 6.11 CPU_ERR_02
    12. 6.12 CPU_ERR_03
    13. 6.13 CPU_ERR_04
    14. 6.14 CRC/CRCP_ERR_01
    15. 6.15 DAC_ERR_01
    16. 6.16 DMA_ERR_01
    17. 6.17 FCC_ERR_01
    18. 6.18 FLASH_ERR_02
    19. 6.19 FLASH_ERR_04
    20. 6.20 FLASH_ERR_05
    21. 6.21 FLASH_ERR_06
    22. 6.22 FLASH_ERR_08
    23. 6.23 GPIO_ERR_01
    24. 6.24 GPIO_ERR_03
    25. 6.25 GPIO_ERR_04
    26. 6.26 GPIO_ERR_06
    27. 6.27 I2C_ERR_01
    28. 6.28 I2C_ERR_02
    29. 6.29 I2C_ERR_03
    30. 6.30 I2C_ERR_04
    31. 6.31 I2C_ERR_05
    32. 6.32 I2C_ERR_06
    33. 6.33 I2C_ERR_07
    34. 6.34 I2C_ERR_08
    35. 6.35 I2C_ERR_09
    36. 6.36 I2C_ERR_10
    37. 6.37 I2C_ERR_13
    38. 6.38 I2C_ERR_15
    39. 6.39 IOMUX_ERR_02
    40. 6.40 MATHACL_ERR_01
    41. 6.41 MATHACL_ERR_02
    42. 6.42 PMCU_ERR_06
    43. 6.43 PMCU_ERR_08
    44. 6.44 PMCU_ERR_10
    45. 6.45 PWREN_ERR_01
    46. 6.46 RST_ERR_01
    47. 6.47 RST_ERR_02
    48. 6.48 RTC_ERR_01
    49. 6.49 SPI_ERR_01
    50. 6.50 SPI_ERR_02
    51. 6.51 SPI_ERR_03
    52. 6.52 SPI_ERR_04
    53. 6.53 SPI_ERR_05
    54. 6.54 SPI_ERR_06
    55. 6.55 SPI_ERR_07
    56. 6.56 SPI_ERR_10
    57. 6.57 SRAM_ERR_02
    58. 6.58 SYSCTL_ERR_02
    59. 6.59 SYSCTL_ERR_03
    60. 6.60 SYSCTL_ERR_04
    61. 6.61 SYSCTL_ERR_05
    62. 6.62 SYSCTL_ERR_06
    63. 6.63 SYSOSC_ERR_01
    64. 6.64 SYSOSC_ERR_02
    65. 6.65 SYSOSC_ERR_04
    66. 6.66 SYSOSC_ERR_05
    67. 6.67 SYSOSC_ERR_06
    68. 6.68 SYSPLL_ERR_01
    69. 6.69 TIMER_ERR_01
    70. 6.70 TIMER_ERR_04
    71. 6.71 TIMER_ERR_06
    72. 6.72 TIMER_ERR_07
    73. 6.73 UART_ERR_01
    74. 6.74 UART_ERR_02
    75. 6.75 UART_ERR_04
    76. 6.76 UART_ERR_05
    77. 6.77 UART_ERR_06
    78. 6.78 UART_ERR_07
    79. 6.79 UART_ERR_08
    80. 6.80 UART_ERR_09
    81. 6.81 UART_ERR_10
    82. 6.82 UART_ERR_11
    83. 6.83 VREF_ERR_01
    84. 6.84 VREF_ERR_02
    85. 6.85 VREF_ERR_04
    86. 6.86 WWDT_ERR_01
    87. 6.87 WWDT_ERR_02
  9.   Trademarks
  10. 7Revision History

Device Nomenclature

To designate the stages in the product development cycle, TI assigns prefixes to the part numbers of all MSP MCU devices. Each MSP MCU commercial family member has one of two prefixes: MSP or XMS. These prefixes represent evolutionary stages of product development from engineering prototypes (XMS) through fully qualified production devices (MSP).

XMS – Experimental device that is not necessarily representative of the final device's electrical specifications

MSP – Fully qualified production device

Support tool naming prefixes:

X: Development-support product that has not yet completed Texas Instruments internal qualification testing.

null: Fully-qualified development-support product.

XMS devices and X development-support tools are shipped against the following disclaimer:

"Developmental product is intended for internal evaluation purposes."

MSP devices have been characterized fully, and the quality and reliability of the device have been demonstrated fully. TI's standard warranty applies.

Predictions show that prototype devices (XMS) have a greater failure rate than the standard production devices. TI recommends that these devices not be used in any production system because their expected end-use failure rate still is undefined. Only qualified production devices are to be used.

TI device nomenclature also includes a suffix with the device family name. This suffix indicates the temperature range, package type, and distribution format.