SLDS272A September 2024 – March 2025 DRV81620-Q1
PRODUCTION DATA
During reverse current (VOUTx_S > VOUTx_D) in high-side configuration or (VOUTx > VMx ), the affected channels stay in ON or in OFF state. Furthermore, during applied reverse currents the ERRx bit can be set if the channel is in ON state and the over temperature threshold is reached.
The general functionality (switch ON and OFF, protection, diagnostic) of unaffected channels is not influenced by reverse currents applied to other channels. Parameter deviations are possible especially for the following ones (Over Temperature protection is not influenced):
Reliability in Limp Home condition for the unaffected channels is unchanged.