SLLA521B January 2022 – June 2022 TCAN1145-Q1 , TCAN1146-Q1
Partial networking is an extremely important function within CAN systems. It allows a reduction of power consumption, which has a direct effect on vehicle emissions. Since there are many applications for partial networking, it is important that any engineer working with CAN is aware of and understands partial networking. This application report serves as an informative guide to any engineer learning partial networking and implementing it using the TCAN1145-Q1 and TCAN1146-Q1.
The benefit of partial networking is to reduce the overall power consumption in the network and is ideal for mixed networks. Because each ECU uses less power while in sleep mode, it benefits the network to only enable needed nodes while the rest are in a low power sleep mode. This is especially important in an automotive setting. Internal combustion engine vehicles use an alternator to recharge their battery and if the vehicle is drawing more power than the alternator can supply, the battery is discharged. This is important when the engine is not running, because sleep mode limits the current and reduces the drain on the battery. The reduced power consumption due to partial networking can have a direct correlation to emissions in vehicles and by reducing the current draw of a car.