SLLSFV9B July 2024 – May 2026 TCAN1473-Q1
PRODMIX
The TCAN1473-Q1 family implements a low-power wake receiver in the standby and sleep mode that uses the multiple filtered dominant wake-up pattern (WUP) defined in the ISO 11898-2:2024 standard.
The WUP is based upon ISO 11898-2, consisting of three parts: a filtered dominant bus, then a filtered recessive bus, followed by a second filtered dominant bus. The first filtered dominant initiates the WUP and the bus monitor is now waiting on a filtered recessive; other bus traffic does not reset the bus monitor. Once a filtered recessive is received, the bus monitor is now waiting on a filtered dominant, and other bus traffic does not reset the bus monitor. Immediately upon receiving of the second filtered dominant, the bus monitor recognizes the WUP.
Once the bus monitor recognizes the WUP, the device drives the RXD terminal low. If a valid VIO is present, the controller is signaled for a wake-up request. If a valid VIO is not present when the wake-up pattern is received, the transceiver drives the RXD output pin low once VIO > UVIOR.
For a dominant or recessive to be considered filtered, the bus must be in that state for more than tWK(FILTER) time. Due to variability in the tWK(FILTER), the following scenarios are applicable. Bus state times less than the tWK(FILTER) minimum are never detected as part of a WUP, and no wake request is generated. Bus state times between tWK(FILTER) minimum and tWK(FILTER) maximum can be detected as part of a WUP and a wake request can be generated. Bus state times more than tWK(FILTER) maximum is always detected as part of a WUP, and a wake request is always generated. See Figure 7-7 for the timing diagram of the WUP.
The pattern and tWK(FILTER) time used for the WUP and wake request prevents noise and bus stuck dominant faults from causing false wake requests while allowing any CAN or CAN FD message to initiate a wake request.
The ISO 11898-2:2024 standard has defined wakeup filter time to enable 1Mbps arbitration.
For an additional layer of robustness and to prevent false wake-ups, the transceiver implements the tWK(TIMEOUT) timer. For a remote wake-up event to successfully occur, the entire wake-up pattern must be received within the timeout value. If the full wake-up pattern is not received before the tWK(TIMEOUT) expires then the internal logic is reset and the transceiver remains in the current mode without waking up. The full pattern must then be transmitted again within the tWK(TIMEOUT) window. See Figure 7-7.
A recessive bus of at least tWK(FILTER) must separate the next WUP pattern if the CAN bus is dominant when the tWK(TIMEOUT) expires.