SLLU348 April 2022 TCAN1167-Q1
The TXD input pin is how messages are transmitted to the bus through the transceiver. TXD can be accessed using the main digital IO jumper. There is an optional pull-up resistor for this signal that may be populated to bias the pin state when the transceiver is not active. There is also a footprint for a filter capacitor if desired by the user.