SLOA198A September 2014 – December 2021 DRV2665 , DRV2667 , DRV2700 , DRV8662
Saturation current is the second-most important parameter of an inductor when using a hysteretic boost converter. Inductor saturation current is typically measured as the peak current that causes the inductance to decrease by 30%. This is the maximum operating current of the inductor.
In Figure 6-1, the saturation current for the 3.3-µH inductor is approximately 400 mA, which is the current that causes the inductance to reduce to 2 µH or by about 30%. A graph like Figure 6-1 can be used to determine and verify the saturation current rating of a specific inductor.
Figure 6-1 Inductance vs DC CurrentThe inductor saturation current value affects two things in the DRV8662, DRV2700, DRV2665, and DRV2667 boost design:
Remember that the current limit on the DRV8662, DRV2665, and DRV2667 is not a safety mechanism, but a threshold to signal when the boost switch should open.
| Tip |
| Often the saturation current is listed on the front page of an inductor datasheet; however, it is good practice to verify this value using an “Inductance vs DC Current” graph similar to Figure 6-1. |