SLOSEB6D February 2025 – November 2025 LMH13000
PRODUCTION DATA
For a stable optical power output in laser drive systems, an APC loop maintains constant performance. Fluctuations in temperature, aging effects, and external conditions introduce variations in laser behavior. An APC loop uses optical feedback to dynamically adjust the current through the laser and keep the optical output fixed.
The following schematic supports both dc and pulsed laser operation by using the laser back-facet photodiode.
When the mux operates in high mode, the APC loop closes, and the optical output from the laser LD tunes so that the current picked up by PD converts into a voltage equal to the VSense voltage across the RS resistance. Adjusting the VREF voltage applied to the TLV9001 error amplifier directly controls the optical power. When the mux operates in low mode, the voltage set by the previous APC closed-loop mode stores across C1. This voltage drives the VSET of LMH13000 and fixes the IOUT at the correct level to deliver the required optical power. The user toggles between low and high modes to periodically correct variations in optical output due to external conditions.
For detailed information, see Automatic Power Control for Laser Diodes Using LMH13000