SLOSEB6D February 2025 – November 2025 LMH13000
PRODUCTION DATA
The LMH13000 is designed to provide a parallel constant current (ICC) at the IOUT. This constant current is in addition to the current set by the VSET. ICC is adjusted by selecting an appropriate RBIAS resistor.
ICC can be set from 4mA to 200mA; IOUT(TOTAL) = ICC, when LVDS = 0 and PD = 0.
For example:
Figure 6-1 shows that the output current IOUT(TOTAL) is the sum of ICC (set by RBIAS) and IOUT which depends on the VSET.
Disable ICC by shorting the RBIAS pin to AVDD. ICC does not depend on the LVDS input. However, during PD = 1 (power-down state), ICC is internally turned off irrespective of the RBIAS value. ICC enables the application to keep a constant current flowing though the connected load. With applications such as laser diode driving, a small bias current such as that of ICC helps improve the optical turn-on time.
Figure 6-1 shows how ICC is dynamically changed by connecting a DAC on the other end of Rfixed resistor.
Equation 3 gives the relation between ICC and VDAC for a given Rfixed resistor connect to RBIAS pin.