SLOSEE6 July 2026 OPA955
ADVANCE INFORMATION
The OPA955 pin layout is optimized to minimize parasitic inductance and capacitance, which is a critical care about in high-speed analog design. The FB pin (pin 1) is internally connected to the output of the amplifier. The FB pin is separated from the inverting input of the amplifier (pin 3) by a no connect (NC) pin (pin 2). The NC pin must be left floating. There are two advantages to this pin layout:
Figure 8-4 RF Connection Between FB and IN– Pins