SLUAAO1 December   2024 BQ27Z746 , BQ27Z758

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Protector Tuning
  5. 2Protector Delay
  6. 3Going to Production With Protector Tuning

Protector Tuning

This section covers how to set the protection values using the protector tuning method.

The protector tuning method does not require any reference voltage to be placed on the device to trim the protections. The expected typical error for UVP and OVP protections is 50mV. The expected typical error for OCC,OCD, and SCD protections is 3mV.

Step 1: Download and install the latest version of BQSTUDIO-TEST.

Step 2: Connect EV2400 with BQ27Z746EVM as in Figure 1-1.

 Hardware Setup Figure 1-1 Hardware Setup

Step 3: Open BQStudio, navigate to the calibration plugin, and select the Protector Tuning Panel.

 Protector Tuning Panel Figure 1-2 Protector Tuning Panel

Step 4: In the Protector Tuning panel, input the desired protection value into the corresponding protection that is being set. A green check mark appears indicating success.

 Protector Tuning
                    Success Figure 1-3 Protector Tuning Success