SLUAAQ7A August 2023 – April 2025 UCC256404
The ZCS happening can occur when the burst packets are too close to each other. This is can happen when there is less off time before coming out of burst mode and the switching node is still ringing which can cause the low side to turn on with current spikes. Figure 4-1 shows how the ZCS problem occurs as burst packets get closer to each other.
Figure 4-1 ZCS Issue Mechanism at Burst Operating Condition