SLUAAS5A November   2025  – June 2026 LMG3427R030 , LMG3427R050

 

  1.   1
  2.   Summary
  3. 1Implementation of LMG3427 in Interleaved TCM PFC
    1. 1.1 Topology of Interleaved TCM PFC
    2. 1.2 ZCD Detection Principle for LMG3427
    3. 1.3 Application Timing for TCM PFC Based on LMG3427
  4. 2ZCD Timing Issue Caused by Inter-phase Capacitance in TCM PFC
    1. 2.1 Inter-phase Parasitic Capacitance Caused by Poor Layout
    2. 2.2 ZCD Timing Issue Caused by Inter-phase Parasitic Capacitance
    3. 2.3 Analysis of ZCD Timing Issue Caused by Inter-phase Capacitance in TCM PFC
  5. 3How to Avoid ZCD Timing Issue Caused by Inter-phase Capacitance During PCB Design
  6. 4Summary
  7. 5References

How to Avoid ZCD Timing Issue Caused by Inter-phase Capacitance During PCB Design

 Remove Overlap Between the First and Second Phases Using External JumpersFigure 3-1 Remove Overlap Between the First and Second Phases Using External Jumpers

The previous analysis reveals that the oscillation in the current flowing through the phase B sync FET actually occurs at the moment phase A is turned on. Through careful analysis of the PCB, we found a large overlap between the switch nodes of phases A and B, which creates a large parasitic capacitance between them. Therefore, when the phase A active FET is turned on, the potential of the phase A switch node changes abruptly, and a large negative current charges this parasitic capacitance, causing the current flowing through the phase B sync FET to actually cross zero. This leads to the ZCD signal being generated prematurely, resulting in ZVS loss. Based on the above analysis, the problem can be solved by removing the overlap between the switch nodes of phases A and B using jumpers.

As shown in Figure 3-2, the ZCD timing issue caused by inter-phase capacitance is resolved when the overlap between phases A and B is removed using jumpers. Therefore, when using the LMG3427, PCB designers need to avoid large overlaps between the switch nodes of each phase.

 Normal Waveform After the Overlap between Phases A and B Is RemovedFigure 3-2 Normal Waveform After the Overlap between Phases A and B Is Removed