SLUAAX9 June   2025 BQ25756

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2MOSFET Power Losses in Buck and Boost Chargers
    1. 2.1 Buck Mode Losses
    2. 2.2 Boost Mode Losses
    3. 2.3 Closing Thoughts for FET Losses
  6. 3Evaluating MOSFETs Using the Design Calculator
    1. 3.1 Correlating MOSFET Data Sheet Parameters With the Design Calculator Parameters
    2. 3.2 Design Calculator MOSFET Comparison Example
  7. 4BOM Evaluation
  8. 5Summary
  9. 6References

Buck Mode Losses

For buck mode, the top FET is the synchronous FET and the bottom FET is the asynchronous FET. The power loss for the top FET can be split into the switching losses and conduction losses and is expressed in Equation 24.

Equation 1. Ptop=Pcon_top+Psw_top

The conduction losses come from the MOSFET being statically-on.

Equation 2. Pcon_top=D×IL_RMS2×RDS(on)_top
Equation 3. IL_RMS2=IL_DC2+Iripple212

The switching losses come from the current and voltage overlap during the FET turn-on and turn-off; the parasitic gate capacitance; and gate drive losses into the FET.

Equation 4. Psw_top=PIV_top+PQoss_top+Pgate_top

Where PIV_top is the loss in the top MOSFET loss due to the current and voltage overlap, PQoss_top is the loss due to the MOSFET parasitic output capacitance, and Pgate_top is the gate drive loss. PIV_top is given by the following equations:

Equation 5. PIV_top=0.5VIN×Ivalley×ton×fsw+0.5VIN×Ipeak×toff×fsw
Equation 6. Ivalley=IL_DC-0.5Iripple
Equation 7. Ipeak=IL_DC+0.5Iripple

Where IL_DC is the DC inductor current and Iripple is the peak-to-peak ripple current of the inductor. The MOSFET turn-on and turn-off times, ton and toff , are defined with the following equations:

Equation 8. ton=Qsw_topIon
Equation 9. toff=Qsw_topIoff

Here, Qsw_top is the switching charge of the top side FET which can be approximated by Equation 10.

Equation 10. Qsw_top=QGD_top+QGS_top

And Ion and Ioff are defined with the following equations:

Equation 11. Ion=VDRV_SUP-VpltRon
Equation 12. Ioff=VpltRoff

Where Vplt is the Miller plateau voltage, VDRV_SUP is the gate drive voltage on the MOSFETs, Ron is the total turn-on gate resistance, and Roff is the total turn-off gate resistance of the gate drive. The next term in the total loss calculation, PQoss_top, can be calculated with Equation 13.

Equation 13. PQoss_top=0.5VIN×Qoss_total×fsw

Where Qoss_total is the total parasitic output charge.

Equation 14. Qoss_total=Qgd_top+Qds_top+Qgd_bot+Qds_bot

The last term in the loss equation can be calculated with Equation 15.

Equation 15. Pgate_top=VIN×Qgate_top×fsw

Where Qgate_top is the gate charge of the top MOSFET and VIN is the input voltage, not the gate drive voltage of the MOSFET. This is to include the losses generated by the internal LDO of the charge controller. If an external gate drive voltage is provided, the LDO losses can be avoided and Equation 16 can be used instead:

Equation 16. Pgate_top=VDRV_SUP×Qgate_top×fsw

The losses for the bottom MOSFET are comprised of conduction losses and switching losses:

Equation 17. Pbottom=Pcon_bottom+Psw_bottom

As for the conduction loss, the loss can be defined for buck mode similar to the top FET with Equation 18.

Equation 18. Pcon_bottom=(1-D)×IL_RMS2×RDS_ON_bottom

Where D is the duty cycle and IL_RMS is the RMS current through the inductor. To minimize the conduction loss, the RDS_ON need to be low. The next and final term in the loss calculation, the switching loss, can be calculated with Equation 28.

Equation 19. Psw_bottom=PRR_bottom+Pdead_bottom+Pgate_bottom

Where the PRR_bottom term is the loss due to the reverse recovery charge of the MOSFET, Pdead_bottom is the loss due to the conduction loss of the body diode during dead time, and Pgate_bottom is the gate drive loss. Each term can be derived with the following equations:

Equation 20. PRR_bottom=VIN×Qrr×fsw
Equation 21. Pdead_bottom=VSD×Ivalley×fsw×tdead_rise+VSD×Ipeak×fsw×tdead_fall
Equation 22. Pgate_bottom=VIN×Qgate_bottom×fsw

Qgate_bottom is the gate charge of the bottom MOSFET, VSD is the forward voltage of the body diode, and VIN is the input voltage, not the gate drive voltage of the MOSFET. This is to include the losses generated by the internal LDO of the device. If an external gate drive voltage is provided, Equation 23 can be used instead:

Equation 23. Pgate_bottom=VDRV_SUP×Qgate_bottom×fsw