SLUAAX9 June   2025 BQ25756

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2MOSFET Power Losses in Buck and Boost Chargers
    1. 2.1 Buck Mode Losses
    2. 2.2 Boost Mode Losses
    3. 2.3 Closing Thoughts for FET Losses
  6. 3Evaluating MOSFETs Using the Design Calculator
    1. 3.1 Correlating MOSFET Data Sheet Parameters With the Design Calculator Parameters
    2. 3.2 Design Calculator MOSFET Comparison Example
  7. 4BOM Evaluation
  8. 5Summary
  9. 6References

Boost Mode Losses

For boost mode, the top FET is asynchronous and the bottom FET is synchronous. The total power losses for the top and bottom FET can be determined in the same way as in buck mode with the following equations:

Equation 24. Ptop=Pcon_top+Psw_top
Equation 25. Pbottom=Pcon_bottom+Psw_bottom

The conduction losses for the top FET are similar the buck mode losses:

Equation 26. Pcon_top=(1-D)×IL_RMS2×RDS(on)_top
Equation 27. IL_RMS2=IL_DC2+Iripple212

In boost mode, the top FET has losses from the reverse recovery charge, dead time, and gate capacitance.

Equation 28. Psw_top=PRR_top+Pdead_top+Pgate_top

The gate losses, dead time losses, and reverse recovery losses are:

Equation 29. PRR_top=VIN×Qrr×fsw
Equation 30. Pdead_top=VSD×Ivalley×fsw×tdead_rise+VSD×Ipeak×fsw×tdead_fall
Equation 31. Pgate_top=VIN×Qgate_top×fsw

As before, if an external gate drive voltage is provided, the following equation can be used instead:

Equation 32. Pgate_top=VDRV_SUP×Qgate_top×fsw

The losses for the bottom FET can be calculated is much the same way as the synchronous buck FET.

Equation 33. Pcon_bottom=D×IL_RMS2×RDS(on)_bottom
Equation 34. IL_RMS2=IL_DC2+Iripple212

The switching losses come from the current and voltage overlap during the FET turn-on and turn-off; the parasitic gate capacitance; and gate drive losses into the FET.

Equation 35. Psw_bottom=PIV_bottom+PQoss_bottom+Pgate_bottom

Where PIV_top is the loss in the top MOSFET loss due to the current and voltage overlap, PQoss_top is the loss due to the MOSFET parasitic output capacitance, and Pgate_top is the gate drive loss. PIV_top is given by the following equations:

Equation 36. PIV_bottom=0.5VIN×Ivalley×ton×fsw+0.5VIN×Ipeak×toff×fsw

The calculations for IValley, IPeak, ton, and toff are the same as in buck mode.