SLUSFV7 November 2024 LMR51403
PRODUCTION DATA
The LMR51403 can also be used to replace asynchronous buck converters, which need a rectifying diode in the application circuit. The design works fine with or without a rectifying diode connected to the switch node of the LMR51403 as shown in the following figure.
Figure 8-2 Replacing Non-Sync Buck Converter