SLUUBH5A November 2016 – February 2022 TPS546C23
The TPS546C23EVM2-746 includes a 49.9-Ω series resistor in the feedback loop for VOUT. The resistor is accessible at the test points TP14 and TP15 for loop response analysis. These test points should be used during loop response measurements as the perturbation injecting points for the loop. See the description in Table 6-1.
| Test Point | Node Name | Description | Comment |
|---|---|---|---|
| TP14 | CHA1 | Input to feedback divider of VOUT | The amplitude of the perturbation at this node should be limited to less than 30 mV. |
| TP15 | CHB1 | Resulting output of VOUT | Bode can be measured by a network analyzer with a CH-B/CH-A configuration. |
Measure only one output at a time with the following procedure: